Increased travel comfort through sustainable and efficient decoupling of lift drive and building foundation
The renovation of lifts is a demanding project. Nowadays, in addition to increased travelling comfort, they should also ensure that the means of transportation is accessible to the handicapped and that they are quiet. The fact that this was successfully achieved in this case, despite having a larger drive in comparison with the previous solution, is also thanks to the ACE rubber-metal isolators. At a natural frequency of 12 to 35 hertz, so-called cup mounts of the type CM-VSC2-40 isolate undesirable vibrations, decouple the new drive from the foundation and thus help to minimise noise to the satisfaction of the people living below the machine room.
Industrial gas springs from ACE are used in order that a heavy wooden gate can be driven easily over uneven ground in front of a shelter for asylum seekers. In...
Premium sauna manufacturer EOS Saunatechnik relies on ACE rubber-metal isolators to eliminate disruptive noises in a sauna whose water for infusions is drawn from a mill wheel. During the...