machines and plants, cladding, panels and flanges, transport systems, offshore industry, oscillation insulation
Saltwater-resistant ACE quick connection elements dampen vibrations, protect against rust penetration and increase the safety of lifeboats
In the present case, when compared to screw connections, the modern quick connection elements produced by ACE have a distinct advantage: their material makes them resistant to the most diverse range of aggressive media, including salt water. Because of this, they provide protection to the housings which encase emergency pressure canisters that are used for the launch of lifeboats. In the most innocuous scenario, the housings would lose their stability through the effects of rust. In the worst case, damage to the pressure canisters could occur or to the entire davit construction.
The maintenance of wind turbines in open seas has long resulted in damage to maintenance boats. Because of impact velocity and swell, an increase in the boat's mass of up to 20 % ...
Saltwater-resistant impact protection for lifeboats
When launching lifeboats, it is theoretically conceivable that there will be contact between the ship and lifeboat. Launching appliances with protective bo...
Driving into lock gates should be specifically facilitated when navigating through Dutch river locks. That is why ACE developed special dampers, based on existing SDP safety shock absorbers but...