FL- No bad vibrations in the sauna, thanks to Flex Locs
FL
Decoupling of pump motors and gears
Flex Locs
Construction
cladding, panels and flanges, oscillation insulation
Isolation of the motor and gearbox of a mill wheel with inexpensive quick connection elements produced by ACE guarantee peace and quiet when taking a sauna
Premium sauna manufacturer EOS Saunatechnik relies on ACE rubber-metal isolators to eliminate disruptive noises in a sauna whose water for infusions is drawn from a mill wheel. During the development phase of the “mill sauna”, it became evident that the motor and gears of the mill wheel drive generated vibrations which were transmitted to the elegant stainless steel housing, and which could have led to uncomfortable noises during continuous operation. The Flex Loc quick connection elements were then installed as a preventative measure and a heavenly peace prevailed in the sauna.
Industrial gas springs from ACE are used in order that a heavy wooden gate can be driven easily over uneven ground in front of a shelter for asylum seekers. In...
The renovation of lifts is a demanding project. Nowadays, in addition to increased travelling comfort, they should also ensure that the means of transportation is accessible to the handicapped and that they ...