Safety damping for the loading mechanics of feeding systems
TUBUS TA
Mech. engineering & automation
z-axes, emergency stop damping in linear axes, linear slides, handling modules, electro-mechanical drives
Inexpensive alternative for avoiding expensive damage in the event of machine failures in feeding systems
Preventing expensive damage after software errors or power outages is the task of two TUBUS TA17-7 profile dampers. Installed in various linear axes, handling and feed systems, they ensure that there are no uncontrolled impacts of the masses in the end positions. Designed as a cost-effective alternative to the hydraulic end position damping length if pinpoint stopping is not a priority, profile dampers demonstrate their strength: High force absorption in a compact design. Thanks to the co-polyester elastomer material, they also outstrip the service life of competing solutions many times over.
Pneumatic linear modules in miniature slide systems ensure high speeds with constant repeat accuracy. In this design, pneumatic end-of-travel damping was deliberately ...
In this design, driven by rodless pneumatic cylinders, two gripper carriages move independently of each other at speeds of 2 to 2.5 m/s. ACE industrial shock absorbers from the produc...
Safety damping for the loading mechanism of lathes
ACE TUBUS profile dampers protect the integrated loading station on a new high speed machining center. The ACE TUBUS damper is designed to prevent overrun on...
ACE miniature shock absorbers optimize production with minimum expenditure. The cycle rate for an assembly line producing electronic components was increased to 3,600 units/...