Saltwater-resistant impact protection for lifeboats
TUBUS TR-L
Marine
shipbuilding, offshore industry, impact or collision protection
Optimum impact protection for rescue boats at sea thanks to saltwater and UV-resistant TUBUS dampers
When launching lifeboats, it is theoretically conceivable that there will be contact between the ship and lifeboat. Launching appliances with protective bodies are fitted in order that the lifeboat is not damaged. Since TUBUS TR-L profile dampers have been doing this job on one of the largest passenger ships in the world, the regular replacement of the damping elements has become a thing of the past. This is because in contrast to earlier solutions made of rubber, the material of the ACE profile dampers does not become brittled or cracked, even in contact with salt water and UV irradiation.
The maintenance of wind turbines in open seas has long resulted in damage to maintenance boats. Because of impact velocity and swell, an increase in the boat's mass of up to 20 % ...
In the present case, when compared to screw connections, the modern quick connection elements produced by ACE have a distinct advantage: their material makes them resistant to the most dive...
Driving into lock gates should be specifically facilitated when navigating through Dutch river locks. That is why ACE developed special dampers, based on existing SDP safety shock absorbers but...