Industrial POWERISE®: ACE Controls Inc. Introduces Actuators to Industrial Applications in the Americas

July 07, 2025

Industrial POWERISE®: ACE Controls Inc. Introduces Actuators to Industrial Applications in the Americas

Industrial POWERISE® is the latest addition to ACE’s comprehensive lineup of engineering solutions. With this launch, ACE Controls Inc. now offers these state-of-the-art linear actuator systems to customers throughout the Americas region, further expanding its portfolio of motion control technologies. As a leader in industrial damping and motion control, ACE can now deliver a brand-new product category—linear actuators—tailored for a wide range of industrial sectors. 

 

With the push of a button, ACE’s Industrial POWERISE® delivers enhanced power and ergonomics to industrial applications—and is perfectly designed to work in combination with ACE gas springs.

 

Following a successful debut in European markets just months ago, Industrial POWERISE® is now enhancing applications across the Americas with greater performance and ergonomic efficiency. With the push of a button, these drives can lift, lower, or precisely position loads using forces from 250 N to 4,000 N. They are capable of automating movement for components such as covers, hoods, doors, gates, and windows, offering flexible spindle pitches from 2 mm to 30 mm and stroke lengths ranging from 50 mm to 350 mm.

 

As automation grows and the demand for user-friendly solutions increases, Industrial POWERISE® meets the need across industries. Whether customers come from ACE’s established base in mechanical engineering or emerging sectors seeking to elevate comfort, control, safety, and precision, this advanced actuator system delivers. From medical technology, manufacturing, and commercial vehicles to aerospace, marine, energy, construction, and furniture, these actuators are purpose-built for today’s industrial environments. 

The system’s roots lie in Automotive POWERISE®—Stabilus’ IATF-certified actuator technology, which has earned global No. 1 OEM leadership in the automotive sector for use in vehicle tailgates and hoods. Now re-engineered for industrial use, Industrial POWERISE® offers flexibility in both vertical and horizontal applications and functions effectively as a positioning system. Its quiet operation—just 55 dB(A)—adds to the overall value, making it an ideal choice for noise-sensitive environments as well.

 

Industrial POWERISE® in Combination with Gas Springs and Engineering Service

 

One of the key differentiators of Industrial POWERISE® in the industrial market is its seamless compatibility with ACE’s NEWTONLINE industrial gas springs. Whether integrated into existing systems that already use gas springs or incorporated into entirely new designs, this combination offers a unique advantage: the actuator provides the dynamic motion, while the gas spring delivers effective load compensation. This synergy not only eases the load on the actuator—allowing for heavier applications and faster travel speeds—but also enhances ergonomics for manual operation. Unlike conventional drive systems, this solution enables manual adjustments without self-locking, ensuring greater flexibility and safety during power failures.

  

 

Industrial POWERISE® linear actuators and ACE’s NEWTONLINE industrial gas springs now operate together on the hoods of CNC machines, significantly enhancing both ergonomics and safety for personnel.

 

With this launch, ACE empowers customers to achieve higher performance, enhanced comfort, and safer automation. Industrial POWERISE® actuators are available as plug-and-play, maintenance-free systems—delivered ready for installation and including control units and accessories—all from a single source. Thanks to a modular design, each system can be easily customized to meet specific application needs, with ACE providing expert support throughout the development process.

 

Available in quantities starting from a single unit, ACE is renowned for its customer–centric engineering, exceptional availability, and top–tier service. For more information, please contact: applications@acecontrols.com for technical questions, customerservice@acecontrols.com for order inquiries and www.acecontrols.com for product details.

Previous Flexibel und anpassungsfähig: Gasfedern für hochwertige und individuelle Lösungen
Next Pack Expo | September 25-26, 2019