Regions Select Region United States of America

Mobile Apps for vibration isolation

Keep it Simple!

In 2014 ACE successfully launched the VibroChecker App. The concept was to create a simple-to-use and self-explanatory mobile tool for the measurement of vibration and shock.

ACE Controls Inc.

The VibroChecker App is available today in three languages as a free installable iOS or Desktop PC app from the Apple Store.

ACE wins automation app award 2014

The VibroChecker PRO is the next logical development step. It's a professional version that allows you to quickly and easily measure vibrations of up to 8,000 Hz. This iOS app can be run on an iPhone or iPad. It still allows you to use the Apple OEM sensors such as accelerometer, gyroscope and microphone which limits measurement to 50 Hz or a professional-grade external sensor for improved results.


VibroChecker PRO

VibroChecker Pro App     +    Digiducer Sensor 333D01

For professional measurements up to 8,000 Hz, an external USB sensor (Digiducer 333D01 - www.digiducer.com) is connected via the Lightning port for Apple products or USB for Desktop PC. The sensor is not included in the price of the app.

The app VibroChecker PRO was developed primarily to provide a professional tool for the measurement of vibration by our technical staff and our partners. The price in the store is a nominal charge for the respective updates.

Core functionalities of the VibroChecker PRO app:

  • 3-axis measurement
  • Variable measuring time
  • Variable start delay 0 to 20 seconds
  • Triggering
  • Select the sampling frequency 10Hz to 100Hz for the internal sensor, 1Hz to 16kHz for external Digiducer sensor
  • Adjustable Auto Repeat function
  • Transmission / storage of measurement data via email as a CSV file

Further information about DIGIDUCER sensor: https://digiducer.com/

After you take a measurement, we are happy to assist you to find appropriate vibration technology solutions. We offer a broad product portfolio with rubber-metal isolators, air springs and vibration isolation pads.
 

×

I have an Account

Secure Orders by encrypted transfer of your data.

I am a new Customer

Wenn Sie in unserem Shop ein Benutzerkonto einrichten, werden Sie schneller durch den Bestellvorgang geführt und genießen unseren individuellen Kundenservice.

  • Vereinfachter Bestellprozess
  • Sicheres Login
  • Individueller Kundenservice

Bitte beachten Sie, dass wir exklusiv an gewerbliche Kunden mit gültiger Umsatzsteuer-Identnummer liefern.